L1380
L1388
L1385
L1390
L1380
L1381
L1382
L1383
L1379.F
L1379.C
Ø | 5 | 10 | 16 | 20 | 25 | 40 | 50 |
16 | • | • | • | ||||
20 | • | • | • | ||||
25 | • | • | • | ||||
32 | • | • | • | ||||
40 | • | • | • | • | |||
50 | • | • | • | ||||
63 | • | • | |||||
80 | • | • |
Ø | 1 | 2 | 3 | 4 | 5 | Nut |
6 | • | flanged | ||||
8 | • | • | • | flanged | ||
10 | • | • | flanged/cylinder | |||
12 | • | • | • | flanged/cylinder | ||
14 | • | flanged/cylinder |
In general it is best to support the ball screws with our ball screw support units (L1388 to L1406) with a fixed end (generally where the motor is mounted) and a floating (support) end. The support units are selected to suit the loads likely to be required, the size of the ball screw (especially its core diameter) and the type of mounting required. Details of the machining required for each end of the ball screw are shown in the bearing mounts technical section.
The data table for the ball screws show the diameter, the lead of the ball screw (i.e. how far the nut travels for one complete revolution of the screw) as well as the mass moment of inertia (also known as the rotational moment of inertia) - this is the extent to which an object resists rotational acceleration about its axis.
Maximum speeds and buckling load data are shown in the technical pages. When using a ball screw the ambient temperature should not exceed +80°C.
During assembly, the parallel alignment of the guides should be ensure. The details on the concentricity of the ball nuts to the ball screws are shown on the technical pages. For linear guideways for use with ball screws please see our part numbers L1016 etc.
Lubrication - the ball screws must be adequately lubricated. This is dependent on load, speed, motion sequence and temperature. Do not use lubricants containing Mo/So or graphite.
In general, the ball nut is already on the ball screw and should not be removed. If you need to machine the ball screw, then the plastic mounting sleeve should be used to retain the ball bearings whilst the nut is removed.
Sometimes ball screws are delivered with a separate ball nut. When mounting the nut on to the screw take care as if done incorrectly the ball bearings may come off the ball nut.
Ball nuts should be mounted only with the help of a plastic mounting sleeve (delivered with the nut). The start of the thread should be aligned so that the seal and the internal parts of the nut are not damaged.
If the balls do unfortunately escape...
If you have any technical queries please call 01483 26 67 74
The maximum axial loads are the loads at which a ball screw will not buckle under compressive loads in the axial direction.
For ease of use the total maximum axial loads are shown in the following graphs.
Factors are:
Apply 50% to the graph figures - to provide a margin of safety.
n1 | n2 | |
Fixed-floating | 2 | 10 |
Fixed-fixed | 4 | 20 |
Fixed-free | 0,25 | 1,3 |
A ball screw of size 40ø. This has a core diameter of 35.8mm.
Distance between the support parts is 600mm.
Using a fixed and floating bearing arrangement.
Reading of graph 1 (fi xed-fl oating) the maximum axial load is going to be 50,000 N (approximately 5 tons).
In the event of variable operating conditions (speed and load), the working life calculations will rely on the average values Fm and nm.
For the average speed nm, in the case of variable speed, apply:
nm = average speed (rpm)
q = time (%)
For the average load Fm, in the case of variable load, apply:
Fm = average load (kN)
q = movement or time at constant speed (%)
For the average load Fm, in the case of both variable load and speed, apply:
Fm = average load (kN)
q = time (%)
nm = average speed (rpm)
Working life L, expressed in revolutions:
L = working life (in rpm)
Fm = average load (kN)
Ca = dynamic load capacity (kN)
Working life L, expressed in hours Lh:
Lh = working life (h)
L = working life (in revolutions)
nm = average speed (r.p.m)
OT = operating time (%)
Output torque Mt, for the transformation of rotational movement into linear movement:
Resistive torque Mr, for the transformation of linear movement into rotational movement:
Mt = output torque (Nm)
Mr = resistive torque (Nm)
F = actual load (kN)
P = pitch (mm)
η = yield (approx. 0.9)
η’ = yield (approx. 0.8)
Output power Pa.
Pa = output power (kW)
Mta = output torque (Nm)
n = speed of rotation (rpm)
(For preloaded double nuts, take no-load torque into account.)
Supported each end by double bearings
Supported each end by single bearings
Supported each end. Double bearings one end, single bearing the other end
Supported one end only by double bearing
As with any rotating shaft a ball screw has a critical speed - which is it’s harmonic vibration.
Critical speed is a function of the diameter and the length of the ball screw, as well as the mounting (support) configuration. The axial clearance of the nut has no influence on the critical speed. We recommend to limit the speed to less than 80% of the critical speed.
The critical speeds are shown in the graphs below.
Supported each end by double bearings
Supported each end by single bearings
Supported each end. Double bearings one end, single bearing the other end
Supported one end only by double bearing
Flange Ø | Max. axial runout |
16-32 | 20 |
32-63 | 25 |
63-125 | 32 |
125-250 | 40 |
250-500 | 50 |
Flange Ø | Max. concentricity error |
16-32 | 20 |
32-63 | 25 |
63-125 | 32 |
125-250 | 40 |
250-500 | 50 |