Cast iron housing
Standard version, passivated and painted Ø12-120mm.
Stainless steel housing
Stainless AISI 304, Ø12-60mm.
Thermoplastic housing
Food grade applications, smooth PBT resin material, Ø20-40mm.
Suitable for:
e.g. food, pharmaceuticals, bottling, outdoor application etc.
Pillow block
Four point flange
Two point flange
Ball bearing units made of stainless steel are used in areas where corrosion resistance is a must. In these areas where high atmospheric humidity or the requirement for periodic washdown of the equipment is necessary to prevent bacteria growth, conventional ball bearing units made of cast iron do not suit.
We off er a comprehensive standard range of ball bearing units made of stainless steel. To satisfy the requirements of the pharmaceutical and food industries all our ball bearing units made of stainless steel are filled with grease meeting the USDA H1 food grade specification.
Pillow block
Four point flange
Two point flange
Self-aligning bearing units must be installed under conditions that ensure maximum bearing life. We recommend that you refer to the following chapters and follow the reference procedures for this type of bearing unit.
When installing sealed bearings, grease the seals to avoid dry operation when the shaft first starts to rotate.
Make sure that the seating surfaces are perfectly clean and flat before starting any installation operations.
Install the shaft by mounting the bearing unit housings on the supporting frame. Tighten the inner ring retaining screw to the required torque indicated in the torque value table.
In all cases the shaft is installed first by attaching the bearing unit housings to the supporting frame. Tighten the screws in alternate diagonals.
The covers (if required) are installed by snap-fitting, which can be done with a light blow of a mallet. They are removed by inserting the tip of a screwdriver into the cavity and applying light pressure to release them.
Tightening of stainless steel fitting screws
M6 thread, torque to 3.9 Nm
M8 thread, torque to 8.3 Nm