The compact rail systems are unique. They have many major advantages over other rail systems.
The rails are easy to set up and can adjust for some misalignment of the structure on which it is being used. The compact rail system achieves this by using a master (T type) rail, and a slave (U type) rail. This allows the sliders in the T rail to remain fixed in place but allows lateral movement of the sliders in the U rail to adapt to any misalignment and avoid any issues of stiction.
Slave (U) rails have flat, parallel raceways that allow free lateral movement of the sliders. This flexibility can mean a large saving in the machining of the structure surface making it a very cost-effective solution.
Fast, smooth and quiet
The unique eccentric roller allows easy preload adjustment for smooth running. Very high speeds allowed, very quiet operation.
Dirt and debris resistant
The internal raceways are resistant to dirt and debris, larger roller bearings with seals and wipers are used (compared to small ball bearings on other systems).
Anti-corrosion option
Alloy coating or nickel plating of the rails and sliders can be applied to provide a corrosion resistant solution.
Rails can be easily joined together for unlimited rail lengths, and extra hole needs to be machined at the joint area. The rails need to be selected so they are “matched” and a joining tool needs to be used to align the rails.
Special purpose & packaging machines
Precision positioning systems
handling units
robotic systems • cutting machines
Seating
Sliding seats
disability ramps
seat extensions
Safety guarding
Extending protective systems
sliding gates
automatic pick & place
Sliding doors & windows
Internal sliding doors
gates • roof lights
display cases
Photography & lighting
Sliding tracks
positioning of lights
shielding systems
Medical technology
X-ray equipment
dental chairs
bed extensions
Food, drink & pharmaceuticals
Food handling conveyors
pharmaceutical factories
stainless display equipment
Transport (naval)
Sliding hatches
pull-out storage
Transport (rail)
Seat adjustment
sliding doors
battery removal units
Transport (automotive)
Ambulance sliding systems
fire fighting vehicles
sliding panels
Transport (military)
Sliding seats
protective hatches
stretcher extensions
The radial load that the sliders can take is significantly higher than the axial load, so where possible the rails should be set up with the sliders taking the loads in this plane.
One of the key benefits of the compact rail system is that it compensates for misalignment in the structure. This often results in a major cost saving when compared to the use of other guideways which have to be very accurately installed.
The compact rail system achieves this by using a master (T type) rail, and a slave (U type) rail. This allows the slides in the T rail to remain fixed in place but allows lateral movement of the sliders in the U rail to adapt to any misalignment and avoid any issues of stiction.
U rails have flat, parallel raceways that allow free lateral movement of the sliders. The maximum lateral movement for each size is shown in later tables.
It is acceptable (but not the preferred method), to use rails as below but the alignment accuracy needed is slightly greater and in this set-up only T type rails can be used.
In this case the axial load figure C0ax should be used in any calculations (which is considerably less than the radial load figure C0rad).
Most of the 3D models (in many formats) are available for download directly from our website www.automotioncomponents.co.uk
Please send us a sketch listing the main points of the application and our Technical Department will deal with this promptly. If required we can also arrange a visit to discuss the application and to show you the different systems available.
The compact rail systems have the following protective coatings as standard:
We can upgrade the anti-corrosion protection of the system by off ering the following:
CS type sliders type NI
Rail and screws