A ball screw is a screw which translates rotary motion into linear motion. Normally used as the driving mechanism in horizontal or vertically driven applications aided by linear guides for supports.
They are described by diameter and pitch or lead. The pitch or lead is the amount of travel you get, or distance the nuts travel along the screw for every complete revolution. They can be operated manually or motorised. They differ from lead screws in that they offer greater precision, speeds, efficiency and accuracy. They are a precision screw which cost considerably more than a lead screw of comparable size so it is important to determine if your application really requires a ball screw. Please contact us if you need any help with this.
For more information or to help determine which products your application requires, please don't hesitate to contact our very friendly sales team.
Rolled ball screws in sizes from 16x5mm up to 80x10mm. Typically stocked in 3000mm lengths but available up to 6000mm.
Wide range of supports including EK, EF, BK, BF, FK, FF, AK, AF and more.
Miniature rolled ball screws and nuts come in 6 -14 mm diameter sizes and with lengths up to 1 metre.
Can be more cost efficient and precise, than running a right-hand ball screw in the reverse direction.


L1380

L1388

L1385

L1390


L1380

L1381

L1382

L1383

L1379.F

L1379.C

Ø | 5 | 10 | 16 | 20 | 25 | 40 | 50 |
| 16 | • | • | • | ||||
| 20 | • | • | • | ||||
| 25 | • | • | • | ||||
| 32 | • | • | • | ||||
| 40 | • | • | • | • | |||
| 50 | • | • | • | ||||
| 63 | • | • | |||||
| 80 | • | • |
Ø | 1 | 2 | 3 | 4 | 5 | Nut |
| 6 | • | flanged | ||||
| 8 | • | • | • | flanged | ||
| 10 | • | • | flanged/cylinder | |||
| 12 | • | • | • | flanged/cylinder | ||
| 14 | • | flanged/cylinder |
In general it is best to support the ball screws with our ball screw support units (L1388 to L1406) with a fixed end (generally where the motor is mounted) and a floating (support) end. The support units are selected to suit the loads likely to be required, the size of the ball screw (especially its core diameter) and the type of mounting required. Details of the machining required for each end of the ball screw are shown in the bearing mounts technical section.
The data table for the ball screws show the diameter, the lead of the ball screw (i.e. how far the nut travels for one complete revolution of the screw) as well as the mass moment of inertia (also known as the rotational moment of inertia) - this is the extent to which an object resists rotational acceleration about its axis.
Maximum speeds and buckling load data are shown in the technical pages. When using a ball screw the ambient temperature should not exceed +80°C.
During assembly, the parallel alignment of the guides should be ensure. The details on the concentricity of the ball nuts to the ball screws are shown on the technical pages. For linear guideways for use with ball screws please see our part numbers L1016 etc.

Lubrication - the ball screws must be adequately lubricated. This is dependent on load, speed, motion sequence and temperature. Do not use lubricants containing Mo/So or graphite.
In general, the ball nut is already on the ball screw and should not be removed. If you need to machine the ball screw, then the plastic mounting sleeve should be used to retain the ball bearings whilst the nut is removed.
Sometimes ball screws are delivered with a separate ball nut. When mounting the nut on to the screw take care as if done
incorrectly the ball bearings may come off the ball nut.

Ball nuts should be mounted only with the help of a plastic mounting sleeve (delivered with the nut). The start of the thread should be aligned so that the seal and the internal parts of the nut are not damaged.
If you have any technical queries please call 01483 26 67 74.
The maximum axial loads are the loads at which a ball screw will not buckle under compressive loads in the axial direction.
For ease of use the total maximum axial loads are shown in the following graphs.
Factors are:
Apply 50% to the graph figures - to provide a margin of safety.

n1 | n2 | |
Fixed-floating | 2 | 10 |
Fixed-fixed | 4 | 20 |
Fixed-free | 0,25 | 1,3 |
A ball screw of size 40ø. This has a core diameter of 35.8mm.
Distance between the support parts is 600mm.
Using a fixed and floating bearing arrangement.
Reading of graph 1 (fi xed-fl oating) the maximum axial load is going to be 50,000 N (approximately 5 tons).
In the event of variable operating conditions (speed and load), the working life calculations will rely on the average values Fm and nm.
For the average speed nm, in the case of variable speed, apply:
nm = average speed (rpm)
q = time (%)
For the average load Fm, in the case of variable load, apply:
Fm = average load (kN)
q = movement or time at constant speed (%)
For the average load Fm, in the case of both variable load and speed, apply:
Fm = average load (kN)
q = time (%)
nm = average speed (rpm)
Working life L, expressed in revolutions:

L = working life (in rpm)
Fm = average load (kN)
Ca = dynamic load capacity (kN)
Working life L, expressed in hours Lh:

Lh = working life (h)
L = working life (in revolutions)
nm = average speed (r.p.m)
OT = operating time (%)
Output torque Mt, for the transformation of rotational movement into linear movement:

Resistive torque Mr, for the transformation of linear movement into rotational movement:

Mt = output torque (Nm)
Mr = resistive torque (Nm)
F = actual load (kN)
P = pitch (mm)
η = yield (approx. 0.9)
η’ = yield (approx. 0.8)
Output power Pa.

Pa = output power (kW)
Mta = output torque (Nm)
n = speed of rotation (rpm)
(For preloaded double nuts, take no-load torque into account.)
Supported each end by double bearings


Supported each end by single bearings.


Supported each end. Double bearings one end, single bearing the other end.


Supported one end only by double bearing


As with any rotating shaft a ball screw has a critical speed - which is it’s harmonic vibration.
Critical speed is a function of the diameter and the length of the ball screw, as well as the mounting (support) configuration. The axial clearance of the nut has no influence on the critical speed. We recommend to limit the speed to less than 80% of the critical speed.
The critical speeds are shown in the graphs below.
Supported each end by double bearings


Supported each end by single bearings


Supported each end. Double bearings one end, single bearing the other end


Supported one end only by double bearing



Flange Ø | Max. axial runout |
| 16-32 | 20 |
| 32-63 | 25 |
| 63-125 | 32 |
| 125-250 | 40 |
| 250-500 | 50 |

Flange Ø | Max. concentricity error |
| 16-32 | 20 |
| 32-63 | 25 |
| 63-125 | 32 |
| 125-250 | 40 |
| 250-500 | 50 |



Designed to withstand or apply high thrust loads with minimum internal friction, ball screws offer a high level of efficiency and positioning accuracy. Ball screws are very well suited for when high accuracy, precision and smooth motion is required and example applications include automotive power steering systems, wind turbines and solar panels.
Ball screws are not self-locking so a break system is required and this should always be factored in. However, ball screws are more efficient and require less torque; having lower friction and being able to run at lower temperatures also helps to reduce footprints.
Ball screws can sometimes experience backlash. However, this issue can be reduced significantly by preselect the ball sizing. There are also times where preloading the ball nut is effective. Please get in touch with one of our expert technical engineers for more help and guidance.