The compact rail system is a unique linear rail, or linear guide system that is very easy to install and allows for some misalignment of the structure in which It is being used. With the pre-load, or stiffness of the system also being adjustable by the user during set up makes this a very user friendly linear system. Induction hardened raceways on all rails and a precision ‘master’ rail ensure this is still a high precision system but with minimal set up time, thus offer cost savings during the installation process.
As specialists in linear motion systems we offer you a choice of materials and sizes. So whether you need lightweight aluminium rails for use in aviation applications or stainless steel components for when exposure to water or corrosive chemicals is a factor, our knowledgable technical engineers are always on hand to provide assistance.
Make sure you download a free Linear Motion Handbook here and utilise our free CAD to help you save time planning your projects.
Light duty, compact rail sliders with rubber seals.
Light duty compact sliders for long linear rails.
Light duty, compact -rails with counterbored fixing holes.
Light duty, compact U-rail with counterbored fixing holes.
Light duty, compact T-rail with countersunk fixing holes.
Light duty, compact U-rail with countersunk fixing holes.
Medium duty compact rail slider. Front fixing with side seal.
Medium duty, compact rail sliders. Front fixing with no side seal.
Medium duty compact rail sliders. Top fixing with side seal.
Medium duty compact rail sliders. Top fixing, size 28. Cast body.
Medium duty, compact U-rails with counterbored holes.
Medium duty compact rails sliders. Front fixing, size 35.
Medium duty compact rail sliders. Front fixing, size 35 without side seal.
Medium duty compact rail sliders. Top fixing, size 35 with side seal.
Heavy duty compact rail sliders. Front fixing, size 43 with side seal.
Heavy duty compact rail sliders. Front fixing, size 43 with no side seal.
Heavy duty compact rail sliders. Top fixing, size 43 with side seal.
Heavy duty compact rail. Top Fixing, size 43. Cast body.
Very heavy duty rail sliders. Front fixing, size 63 with no side seal.
Very heavy duty compact slider. Top fixing, size 63. Cast body.
Very heavy duty compact T-rails with counterbored holes.
Very heavy duty compact T-rails with countersunk holes.
Very heavy duty compact U-rails with countersunk holes.
Very heavy duty compact K-rails with counterbored holes.
Very heavy duty compact K-rails with countersunk holes.
Inidivdual rollers for use with our compact rail system products.
The radial load that the sliders can take is significantly higher than the axial load, so where possible the rails should be set up with the sliders taking the loads in this plane.
One of the key benefits of the compact rail system is that it compensates for misalignment in the structure. This often results in a major cost saving when compared to the use of other guideways which have to be very accurately installed.
The compact rail system achieves this by using a master (T type) rail, and a slave (U type) rail. This allows the slides in the T rail to remain fixed in place but allows lateral movement of the sliders in the U rail to adapt to any misalignment and avoid any issues of stiction.
U rails have flat, parallel raceways that allow free lateral movement of the sliders. The maximum lateral movement for each size is shown in later tables.
It is acceptable (but not the preferred method), to use rails as below but the alignment accuracy needed is slightly greater and in this set-up only T type rails can be used.
In this case the axial load figure C0ax should be used in any calculations (which is considerably less than the radial load figure C0rad).
Most of the 3D models (in many formats) are available for download directly from our website www.automotioncomponents.co.uk
Please send us a sketch listing the main points of the application and our Technical Department will deal with this promptly. If required we can also arrange a visit to discuss the application and to show you the different systems available.
The compact rail systems have the following protective coatings as standard:
We can upgrade the anti-corrosion protection of the system by off ering the following:
CS type sliders type NI
Rail and screws